AXIS#.VL.KIMODE

Description

This parameter sets whether the velocity mode is:

0 – Always on

1 – On ONLY if the position loop integrator is inactive.

AXIS#.PL.KITHRESH can be used to set a velocity command threshold to control at what part of a move the position loop integrator is active. When the position loop integrator becomes inactive, the velocity loop integrator will become active.

Usage

As a general rule, AXIS#.PL.KI should not be used at the same time as AXIS#.VL.KI , the two integrators will oppose each other and likely cause undesirable results, sometimes a runaway. Using AXIS#.PL.KITHRESH in conjunction with AXIS#.VL.KIMODE the user can specify operating conditions to switch between integrators based on machine operation.

Often times it makes sense to use the velocity integrator during a move, but as the motion comes to an end, to switch back to the position integrator for fine positioning.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.KIMODE

5011h

25h

Unsigned8

-

-

Read/Write

No

AXIS2.VL.KIMODE

5111h

25h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6042

1

6042 (0x179a)

AXIS1.VL.KIMODE

Unsigned8

Read/Write

Yes

71578

2

6042 (0x179a)

AXIS2.VL.KIMODE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KIMODE

6042

Unsigned8

Read/Write

-